iMX6 framebuffer error with yocto

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 framebuffer error with yocto

Jump to solution
1,972 Views
krisztianbakos
Contributor II

Hello,

I have a strange error with my custom iMX6 board, running Yocto -> fido | meta-qt5 -> fido.

The framebuffer device comes up and I see picture on my LCD screen, but after some minutes I get the following error:

root@imx6qsabresd:~# imx-ipuv3 2400000.ipu: ch = 9, pm_runtime_put failed:-38!

CPU: 0 PID: 25 Comm: kworker/0:1 Not tainted 3.14.28-1.0.0_ga+g91cf351 #7

Workqueue: events console_callback

[<80014644>] (unwind_backtrace) from [<8001164c>] (show_stack+0x10/0x14)

[<8001164c>] (show_stack) from [<8065485c>] (dump_stack+0x7c/0xbc)

[<8065485c>] (dump_stack) from [<80459cdc>] (ipu_uninit_channel+0x524/0xa7c)

[<80459cdc>] (ipu_uninit_channel) from [<802ca220>] (mxcfb_blank+0x80/0xb8)

[<802ca220>] (mxcfb_blank) from [<802b0550>] (fb_blank+0x54/0xa8)

[<802b0550>] (fb_blank) from [<802ba92c>] (fbcon_blank+0xf4/0x2a8)

[<802ba92c>] (fbcon_blank) from [<802f6604>] (do_blank_screen+0x1d4/0x284)

[<802f6604>] (do_blank_screen) from [<802f94dc>] (console_callback+0x88/0x15c)

[<802f94dc>] (console_callback) from [<8003ed2c>] (process_one_work+0xf4/0x35c)

[<8003ed2c>] (process_one_work) from [<8003f97c>] (worker_thread+0x130/0x3bc)

[<8003f97c>] (worker_thread) from [<80044c3c>] (kthread+0xcc/0xe4)

[<80044c3c>] (kthread) from [<8000e478>] (ret_from_fork+0x14/0x3c)

And my screen goes off (pixel clock stops)

Does anyone have any idea what could be the problem?

Thank you in advance!

Best regards,

Krisztián Bakos

Labels (4)
0 Kudos
Reply
1 Solution
1,655 Views
krisztianbakos
Contributor II

Hello Alfred,

Thank you for the answer. The thing is, that the power management was disabled in the Kernel, thus it could not switch power states. I re-enabled it and now it works fine. However, this was not such a huge issue as I could re-enable the screen (turned out it was the "screensaver"... -.-')

Best Regards,

Krisztián

View solution in original post

0 Kudos
Reply
2 Replies
1,655 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Krisztian,

It looks like you are getting some external exception and it is not handle correctly, you can check your dtsi files, for the default_ifmt and the pinctrl.

Hope this helps

0 Kudos
Reply
1,656 Views
krisztianbakos
Contributor II

Hello Alfred,

Thank you for the answer. The thing is, that the power management was disabled in the Kernel, thus it could not switch power states. I re-enabled it and now it works fine. However, this was not such a huge issue as I could re-enable the screen (turned out it was the "screensaver"... -.-')

Best Regards,

Krisztián

0 Kudos
Reply