i.MX53 VPU decoder output timing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX53 VPU decoder output timing

Jump to solution
1,685 Views
torus1000
Contributor V

Hi Chip experts,

I have a quesion when i.MX53 VPU decoded data write to the frame buffer.

Which timing is correct?

a)  data wrote per each microblock decoded
b)  or data wrote only when whole frame decoded

Thanks.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,581 Views
joanxie
NXP TechSupport
NXP TechSupport

The VPU has an internal DSP called the BIT processor which controls the internal hardware blocks for

video decoder operations.

The BIT processor completes decoding operations on a frame-by-frame basis, which allows low level

independency of VPU operations to the host processor

View solution in original post

0 Kudos
Reply
1 Reply
1,582 Views
joanxie
NXP TechSupport
NXP TechSupport

The VPU has an internal DSP called the BIT processor which controls the internal hardware blocks for

video decoder operations.

The BIT processor completes decoding operations on a frame-by-frame basis, which allows low level

independency of VPU operations to the host processor

0 Kudos
Reply