iMX6 battery boot problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6 battery boot problem

1,707件の閲覧回数
joseporga
Contributor I

We have boot problems in SABRE SD platform after halting system while having LICELL pin connected to a coin cell battery (BT500 connector in SABRE SD platform).

The steps we have followed are:

  1. Connect a coin cell battery to BT500 SABRE SD platform connector.
  2. Switch SABRE SD platform board on.
  3. Boot linux and enter commands to refresh date:
    • date -s '2016-04-27 18:34:00'
    • hwclock -w
  4. Enter halt command:
    • halt
  5. Switch SABRE SD platform board off and on.

After following these steps we are not able to boot the SABRE SD platform anymore. To be able to boot the board, we have to disconnect the coin cell battery.

If step 4 is not applied (no halt command is introduced) we have no booting problems.

Why are we having this issue?

ラベル(6)
0 件の賞賛
返信
1 返信

1,487件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Looks like, the problem relates to PMIC settings after Linux "halt" command,

which do not allow to start-up system : full POR reset is needed (to return default

PMIC configuration).

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信