iMX6_SOLOX_3V3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX6_SOLOX_3V3

跳至解决方案
1,866 次查看
victorafanasiev
Contributor II

My questions are concerning of powering the microprocessor   iMX6 SOLOX from a 3.3 volts input power source. For power sequencing I use the preprogrammed PMIC chip MMPF0200F6AEP. But I would like not to use the SW2 output of the PMIC as a source of 3.3 volts for my PCB. I plan to use the input voltage and a load switch instead of use the SW2 output of the PMIC. To control of the load switch I want to use the output voltage of the SW3A output of the PMIC. Is it correct using of PMIC? If so, may I leave unconnected the pins SW2LX, SW2IN, SW2FB of the PMIC chip MMPF0200F6AEP? Or I must connect them as in the MCIMX6SX SDB board  (SCH-27962)? Is it mandatory to have 3.3 volts on the SW2 output for correct operation the chip MMPF0200F6AEP?

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,718 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Viktor

for unused pins connection one can look at

Table 1. MMPF0200 pin connection guidelines AN4751 Schematic guidelines for the MMPF0200

https://www.nxp.com/docs/en/application-note/AN4751.pdf 

yes one can use external (not pmic) power for processor, provided that

power-up sequence is followed (it is described in i.MX6SX Datasheet).

https://www.nxp.com/docs/en/data-sheet/IMX6SXCEC.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,719 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Viktor

for unused pins connection one can look at

Table 1. MMPF0200 pin connection guidelines AN4751 Schematic guidelines for the MMPF0200

https://www.nxp.com/docs/en/application-note/AN4751.pdf 

yes one can use external (not pmic) power for processor, provided that

power-up sequence is followed (it is described in i.MX6SX Datasheet).

https://www.nxp.com/docs/en/data-sheet/IMX6SXCEC.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复