iMX6_SOLOX_3V3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6_SOLOX_3V3

Jump to solution
1,897 Views
victorafanasiev
Contributor II

My questions are concerning of powering the microprocessor   iMX6 SOLOX from a 3.3 volts input power source. For power sequencing I use the preprogrammed PMIC chip MMPF0200F6AEP. But I would like not to use the SW2 output of the PMIC as a source of 3.3 volts for my PCB. I plan to use the input voltage and a load switch instead of use the SW2 output of the PMIC. To control of the load switch I want to use the output voltage of the SW3A output of the PMIC. Is it correct using of PMIC? If so, may I leave unconnected the pins SW2LX, SW2IN, SW2FB of the PMIC chip MMPF0200F6AEP? Or I must connect them as in the MCIMX6SX SDB board  (SCH-27962)? Is it mandatory to have 3.3 volts on the SW2 output for correct operation the chip MMPF0200F6AEP?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,749 Views
igorpadykov
NXP Employee
NXP Employee

Hi Viktor

for unused pins connection one can look at

Table 1. MMPF0200 pin connection guidelines AN4751 Schematic guidelines for the MMPF0200

https://www.nxp.com/docs/en/application-note/AN4751.pdf 

yes one can use external (not pmic) power for processor, provided that

power-up sequence is followed (it is described in i.MX6SX Datasheet).

https://www.nxp.com/docs/en/data-sheet/IMX6SXCEC.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,750 Views
igorpadykov
NXP Employee
NXP Employee

Hi Viktor

for unused pins connection one can look at

Table 1. MMPF0200 pin connection guidelines AN4751 Schematic guidelines for the MMPF0200

https://www.nxp.com/docs/en/application-note/AN4751.pdf 

yes one can use external (not pmic) power for processor, provided that

power-up sequence is followed (it is described in i.MX6SX Datasheet).

https://www.nxp.com/docs/en/data-sheet/IMX6SXCEC.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply