iMX6 SDMA Function

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,637件の閲覧回数
koichisakagami
Contributor II

Dear Sirs,
I would like to use the scatter/gather function between SDIO and memorys.

Does iMX6 SDMA support  scatter/gather function between SDIO and memorys ?
Or ,do I have to use the internal DMA ( in uSDHC module) ?


If Yes, does the Linux BSP support above function ?

Best Regards,

Koichi Sakagami

ラベル(2)
0 件の賞賛
返信
1 解決策
2,154件の閲覧回数
Rhyme
Contributor III

Dear Koichi-san,

Are you asking

(1) Does SDMA support scatter/gather function?

(2) Does SDMA support transfer biween memory and SDIO?

If (1) is the case, Assuming the "scatter/gather" means

similar function in eDMA, SDMA seems to have superior function(s).

Please refer to the chapter of SDMA in RM.

If (2) is the case, most probably the answer is yes,

but I think that you need to describe what you'd like to

accomplish more specifically to get appropriate answer(s).

Best Regards,

4-Feb-2014

Motoo Tanaka

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,155件の閲覧回数
Rhyme
Contributor III

Dear Koichi-san,

Are you asking

(1) Does SDMA support scatter/gather function?

(2) Does SDMA support transfer biween memory and SDIO?

If (1) is the case, Assuming the "scatter/gather" means

similar function in eDMA, SDMA seems to have superior function(s).

Please refer to the chapter of SDMA in RM.

If (2) is the case, most probably the answer is yes,

but I think that you need to describe what you'd like to

accomplish more specifically to get appropriate answer(s).

Best Regards,

4-Feb-2014

Motoo Tanaka

0 件の賞賛
返信
2,154件の閲覧回数
koichisakagami
Contributor II

Dear Tanaka-san,

Thank you for reply.

It is (2) that I would like to ask.

I understood. I post the questions more specifically.

Best Regards,

Koichi sakagami

0 件の賞賛
返信