iMX6 SDMA Function

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 SDMA Function

Jump to solution
2,683 Views
koichisakagami
Contributor II

Dear Sirs,
I would like to use the scatter/gather function between SDIO and memorys.

Does iMX6 SDMA support  scatter/gather function between SDIO and memorys ?
Or ,do I have to use the internal DMA ( in uSDHC module) ?


If Yes, does the Linux BSP support above function ?

Best Regards,

Koichi Sakagami

Labels (2)
0 Kudos
Reply
1 Solution
2,200 Views
Rhyme
Contributor III

Dear Koichi-san,

Are you asking

(1) Does SDMA support scatter/gather function?

(2) Does SDMA support transfer biween memory and SDIO?

If (1) is the case, Assuming the "scatter/gather" means

similar function in eDMA, SDMA seems to have superior function(s).

Please refer to the chapter of SDMA in RM.

If (2) is the case, most probably the answer is yes,

but I think that you need to describe what you'd like to

accomplish more specifically to get appropriate answer(s).

Best Regards,

4-Feb-2014

Motoo Tanaka

View solution in original post

0 Kudos
Reply
2 Replies
2,201 Views
Rhyme
Contributor III

Dear Koichi-san,

Are you asking

(1) Does SDMA support scatter/gather function?

(2) Does SDMA support transfer biween memory and SDIO?

If (1) is the case, Assuming the "scatter/gather" means

similar function in eDMA, SDMA seems to have superior function(s).

Please refer to the chapter of SDMA in RM.

If (2) is the case, most probably the answer is yes,

but I think that you need to describe what you'd like to

accomplish more specifically to get appropriate answer(s).

Best Regards,

4-Feb-2014

Motoo Tanaka

0 Kudos
Reply
2,200 Views
koichisakagami
Contributor II

Dear Tanaka-san,

Thank you for reply.

It is (2) that I would like to ask.

I understood. I post the questions more specifically.

Best Regards,

Koichi sakagami

0 Kudos
Reply