iMX6 RGMII level

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
6,048件の閲覧回数
tarterkit_ru
Contributor III

Datasheet have "RGMII I/O supply voltage: 1.14 - 1.5 - 1.9V"

But as i know, some boards with iMX6 have  KSZ9021RN ethernet PHY and it have RGMII IO 2.5/3.3V

I can't find datasheet of AR8031 for understanding how RGMII IO supply in development board, but as i know RGMII IO 1.5-1.8V it only for RGMII V2.0 specification but brief pdf of  AR8031 dont have RGMII V2.0

What volages can be supply to   RGMII I/O?

ラベル(1)
0 件の賞賛
返信
1 解決策
3,663件の閲覧回数
david_babin
NXP Employee
NXP Employee

The new MX6 data sheet on extranet shows RGMII I/O supply voltage range 1.15 - 2.625 V. So, MX6 is very flexible. The supply voltage you use depends on the PHY. With AR8031, use 1.5 V for the I/O supply. With KSZ9021, use 2.5 V on the I/O supply.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,664件の閲覧回数
david_babin
NXP Employee
NXP Employee

The new MX6 data sheet on extranet shows RGMII I/O supply voltage range 1.15 - 2.625 V. So, MX6 is very flexible. The supply voltage you use depends on the PHY. With AR8031, use 1.5 V for the I/O supply. With KSZ9021, use 2.5 V on the I/O supply.

0 件の賞賛
返信
3,663件の閲覧回数
zhanghan
Contributor II

hello  if  i use 1.8V at PHY ,then i should use 1.8V at imx6 ,I want to communicate via RJ45 as pic below.

frame.png

but i find  when i use  1.8V ,the bit of MODE[2] Rxclk should be 1 as pic below.

1V8.png

That is the mode is x1xx,and there is no mode  can access 1000M speed。MODE.png

Am I wrong?What should I do?

0 件の賞賛
返信
3,663件の閲覧回数
rveer
Contributor II

Hi David,

I am facing same clock issue with custom iMX6 board where an marvell switch is connected via RGMII.could you please suggest me, how can I configure to increase voltage from 1.8V to 2.5 V on RGMII line from SoC side?.


Regards

Raj


https://community.nxp.com/message/339730/edit" style="font-style: inherit; font-family: inherit; col...

0 件の賞賛
返信
3,664件の閲覧回数
tarterkit_ru
Contributor III

Great!
Thanks!

0 件の賞賛
返信