iMX6_PowerConsumption

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6_PowerConsumption

ソリューションへジャンプ
1,693件の閲覧回数
bordeaujean-pas
Contributor I

Hello,

I would like to analyse power consumption with a SABRESD following the AN4509.pdf

I haven't found the several audio/video files used in the application note...

- 128kbps_44khz_s_mp3.mp3

- mxc_vpu_test.out

- 3DMARK_es11

- H264_ML_1920x1080_10Mbps_15fps_noaudio.h264

- fsl-clip-1080p.h264

Does somebody know where to found them?

Regards.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,589件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi BORDEAU

imx-test package can be found on

http://repository.timesys.com/buildsources/i/imx-test/imx-test-3.0.35-4.0.0/

some test clips are proprietary and can not be distributed, sorry.

However one can find other test streams on web or use for example

Codecs and other Algorithms (3)

Multimedia test streams for the i.MX27 ADS platform. (REV 1.1)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,590件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi BORDEAU

imx-test package can be found on

http://repository.timesys.com/buildsources/i/imx-test/imx-test-3.0.35-4.0.0/

some test clips are proprietary and can not be distributed, sorry.

However one can find other test streams on web or use for example

Codecs and other Algorithms (3)

Multimedia test streams for the i.MX27 ADS platform. (REV 1.1)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信