iMX6_PowerConsumption

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6_PowerConsumption

Jump to solution
1,695 Views
bordeaujean-pas
Contributor I

Hello,

I would like to analyse power consumption with a SABRESD following the AN4509.pdf

I haven't found the several audio/video files used in the application note...

- 128kbps_44khz_s_mp3.mp3

- mxc_vpu_test.out

- 3DMARK_es11

- H264_ML_1920x1080_10Mbps_15fps_noaudio.h264

- fsl-clip-1080p.h264

Does somebody know where to found them?

Regards.

Labels (1)
0 Kudos
Reply
1 Solution
1,591 Views
igorpadykov
NXP Employee
NXP Employee

Hi BORDEAU

imx-test package can be found on

http://repository.timesys.com/buildsources/i/imx-test/imx-test-3.0.35-4.0.0/

some test clips are proprietary and can not be distributed, sorry.

However one can find other test streams on web or use for example

Codecs and other Algorithms (3)

Multimedia test streams for the i.MX27 ADS platform. (REV 1.1)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,592 Views
igorpadykov
NXP Employee
NXP Employee

Hi BORDEAU

imx-test package can be found on

http://repository.timesys.com/buildsources/i/imx-test/imx-test-3.0.35-4.0.0/

some test clips are proprietary and can not be distributed, sorry.

However one can find other test streams on web or use for example

Codecs and other Algorithms (3)

Multimedia test streams for the i.MX27 ADS platform. (REV 1.1)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply