Hi everyone,
The board that I design has not the PMIC for iMX6.
So, I will configure as follows.
 12V@3A     ---> 5V@3A(DCDC)     ---> 3.0V@300mA(LDO) - VSNVS_IN & VDDHIGH_IN (1)
                    |                                    ---> 1.375V@2.5A(DCDC)- ARM_IN   (2)
                    |                                    ---> 1.375V@2.5A(DCDC)- VDDSOC_IN  (2)
                    |
                    |          
                    |---> 5V@3A(DCDC)   ---> 1.5V@1.5A(DCDC)- DDR3 (3) 
                                                        ---> 3.3V@1.5A(DCDC)- IOs  (4)
                    "(x)" is a power sequence.
 
Powers will be controlled as follows
 (1)powergood => (2)enable =>  (2)powergood(or voltage supervisor ic) => POR & (3)enable =>  (3)powergood => (4)enable.
 
Is this power configuration OK?
Thanks.
已解决! 转到解答。
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi chilwonna
I think power up sequence is good. POR should be asserted from
beginning and deasserted when all power supplies and 24MHz/32.768KHz
clocks become stable.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi chilwonna
I think power up sequence is good. POR should be asserted from
beginning and deasserted when all power supplies and 24MHz/32.768KHz
clocks become stable.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
Recently I was working on i.MX6 DL sabreSD board without PMIC.
For software issue, What configuration did you modified?
Did I need to modify some driver myself or I just need to set all the configuration which related with Power Management to disabled?
Thanks in advanced!