Hi NXP team,
We are working on iMX6ULL and PCAL6416 GPIO expander on Linux 4.14.98. The /linux/drivers/gpio/gpio-pca953x.c driver is backported from Linux 5.2
Currently the pcal6416 gpio controller function is OK. From iMX6 gpio 1 pin 6 use as the gpio pin to receive the pcal6416 interrupt signal.
We expected to use the interrupt from the pcal6416 as interrupt expander and the device tree as below:
&i2c1 {
	clock-frequency = <100000>;
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_i2c1>;
	status = "okay";
	exp_gpio1: exp_gpio1@20 {
		compatible = "nxp,pcal6416";
		reg = <0x20>;
		gpio-controller;
		#gpio-cells = <2>;
		status = "okay";
		reset-gpios = <&gpio5 6 GPIO_ACTIVE_HIGH>;
		vcc-supply = <®_sd1_vmmc>;
		interrupt-parent = <&gpio1>;
		interrupts = <6 IRQ_TYPE_EDGE_FALLING>;
		interrupt-controller;
		#interrupt-cells = <2>;
	};
With the device tree configuration as above the issue has occurred. From the debug console after "Starting kernel ..." line is printed kernel hang and it needs up to 30 minutes to boot up and IRQ init for pcal6416 is OK.
Could you please help me to clarify any issue from the device tree configuration or any workaround for this.
Thanks in advance,
Phuong Nguyen
已解决! 转到解答。
I can recommend you that you verify that you Interrupt ID, it is correct always take in consideration that the Interrupts are 32 bits Shift.
And you can take a look to the Kernel Documentation regarding the device tree configuration
https://www.kernel.org/doc/Documentation/devicetree/bindings/interrupt-controller/interrupts.txt
I can recommend you that you verify that you Interrupt ID, it is correct always take in consideration that the Interrupts are 32 bits Shift.
And you can take a look to the Kernel Documentation regarding the device tree configuration
https://www.kernel.org/doc/Documentation/devicetree/bindings/interrupt-controller/interrupts.txt