iMX6 - PCAL6416 - Linux kernel gpio expander interrupt issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6 - PCAL6416 - Linux kernel gpio expander interrupt issue

ソリューションへジャンプ
4,483件の閲覧回数
vocsiphuong
Contributor I

Hi NXP team,

We are working on iMX6ULL and PCAL6416 GPIO expander on Linux 4.14.98. The /linux/drivers/gpio/gpio-pca953x.c driver is backported from Linux 5.2

Currently the pcal6416 gpio controller function is OK. From iMX6 gpio 1 pin 6 use as the gpio pin to receive the pcal6416 interrupt signal.

We expected to use the interrupt from the pcal6416 as interrupt expander and the device tree as below:

 

 

 

&i2c1 {
	clock-frequency = <100000>;
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_i2c1>;
	status = "okay";

	exp_gpio1: exp_gpio1@20 {
		compatible = "nxp,pcal6416";
		reg = <0x20>;
		gpio-controller;
		#gpio-cells = <2>;
		status = "okay";
		reset-gpios = <&gpio5 6 GPIO_ACTIVE_HIGH>;
		vcc-supply = <&reg_sd1_vmmc>;

		interrupt-parent = <&gpio1>;
		interrupts = <6 IRQ_TYPE_EDGE_FALLING>;
		interrupt-controller;
		#interrupt-cells = <2>;
	};

 

 

 

With the device tree configuration as above the issue has occurred. From the debug console after "Starting kernel ..." line is printed kernel hang and it needs up to 30 minutes to boot up and IRQ init for pcal6416 is OK.

Could you please help me to clarify any issue from the device tree configuration or any workaround for this.

Thanks in advance,

Phuong Nguyen

0 件の賞賛
返信
1 解決策
4,447件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

I can recommend you that you verify that you Interrupt ID, it is correct always take in consideration that the Interrupts are 32 bits Shift.

And you can take a look to the Kernel Documentation regarding the device tree configuration

 

https://www.kernel.org/doc/Documentation/devicetree/bindings/interrupt-controller/interrupts.txt

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,552件の閲覧回数
5454ty
Contributor II

HI,

   I am debugging the pcal6416,and can you share the linux driver . thank you 

0 件の賞賛
返信
4,448件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

I can recommend you that you verify that you Interrupt ID, it is correct always take in consideration that the Interrupts are 32 bits Shift.

And you can take a look to the Kernel Documentation regarding the device tree configuration

 

https://www.kernel.org/doc/Documentation/devicetree/bindings/interrupt-controller/interrupts.txt

 

 

0 件の賞賛
返信