iMX6 NAND Address cycles definition

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6 NAND Address cycles definition

ソリューションへジャンプ
4,813件の閲覧回数
tarterkit_ru
Contributor III

Reference Manual have:

Table 8-11. NAND Boot eFUSE Descriptions: BOOT_CFG1[1:0] - Address Cycles

Fusemap Table 5-8. NAND Boot Fusemap: BOOT_CFG1[1:0] - Nand_Row_address_byte

What exactly need set to BOOT_CFG[1:0], all address cycles or only row address cycles?

ラベル(2)
1 解決策
3,931件の閲覧回数
Yuri
NXP Employee
NXP Employee

It looks like AddressCycles are Row Address Bytes, assuming Column Address Bytes = 2 

元の投稿で解決策を見る

5 返答(返信)
3,931件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

It should be all address cycles.

Regards,

Weidong

0 件の賞賛
返信
3,931件の閲覧回数
Rodrigue
NXP Employee
NXP Employee

Hi Weidong,

Are you sure? because the fuse map definition we use to have specifies the NAND row address bytes.

May you please confirm?

regards,

0 件の賞賛
返信
3,932件の閲覧回数
Yuri
NXP Employee
NXP Employee

It looks like AddressCycles are Row Address Bytes, assuming Column Address Bytes = 2 

3,931件の閲覧回数
_timm
Contributor II

Hi: did we ever reach a definitive conclusion on this? I have the exact same situation: an OEM has set these fuses to 11b, but the NAND device that we are using has 2 column address bytes (fuses are 00b according to DQRM). So what is the correct answer? 

Thanks,

Tim Meese

0 件の賞賛
返信
3,931件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   The recent i.MX6 D/Q RM (IMX6DQRM, Rev. 3, 07/2015) clearly states in both tables,
that BOOT_CFG1[1:0] field defines  Row Address Cycles.

Table 5-9 (NAND Boot Fusemap)

Table 8-10 (NAND Boot eFUSE Descriptions)

http://www.nxp.com/assets/documents/data/en/reference-manuals/IMX6DQRM.pdf 

Regards,

Yuri.