iMX6 NAND Address cycles definition

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX6 NAND Address cycles definition

跳至解决方案
4,829 次查看
tarterkit_ru
Contributor III

Reference Manual have:

Table 8-11. NAND Boot eFUSE Descriptions: BOOT_CFG1[1:0] - Address Cycles

Fusemap Table 5-8. NAND Boot Fusemap: BOOT_CFG1[1:0] - Nand_Row_address_byte

What exactly need set to BOOT_CFG[1:0], all address cycles or only row address cycles?

标签 (2)
1 解答
3,947 次查看
Yuri
NXP Employee
NXP Employee

It looks like AddressCycles are Row Address Bytes, assuming Column Address Bytes = 2 

在原帖中查看解决方案

5 回复数
3,947 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

It should be all address cycles.

Regards,

Weidong

0 项奖励
回复
3,947 次查看
Rodrigue
NXP Employee
NXP Employee

Hi Weidong,

Are you sure? because the fuse map definition we use to have specifies the NAND row address bytes.

May you please confirm?

regards,

0 项奖励
回复
3,948 次查看
Yuri
NXP Employee
NXP Employee

It looks like AddressCycles are Row Address Bytes, assuming Column Address Bytes = 2 

3,947 次查看
_timm
Contributor II

Hi: did we ever reach a definitive conclusion on this? I have the exact same situation: an OEM has set these fuses to 11b, but the NAND device that we are using has 2 column address bytes (fuses are 00b according to DQRM). So what is the correct answer? 

Thanks,

Tim Meese

0 项奖励
回复
3,947 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   The recent i.MX6 D/Q RM (IMX6DQRM, Rev. 3, 07/2015) clearly states in both tables,
that BOOT_CFG1[1:0] field defines  Row Address Cycles.

Table 5-9 (NAND Boot Fusemap)

Table 8-10 (NAND Boot eFUSE Descriptions)

http://www.nxp.com/assets/documents/data/en/reference-manuals/IMX6DQRM.pdf 

Regards,

Yuri.