iMX6 MIPI error info

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6 MIPI error info

2,764件の閲覧回数
ashokp
Contributor I

Hi All,

Please let me know is it possible to check the following error in imx6 MIPI interface.

1.Total number of frames received

2. Number of packets with CRC errors

3. Number of frames dropped because of buffer under run

4. Number of frames that were not completed

5. Frames per second

Thanks,

P.Ashok

ラベル(3)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,590件の閲覧回数
ashokp
Contributor I

Hi ,

I am using MIPI_CSI interface and nitrogen 6x board with ubuntu 3.14.2 kernel version. Please update me the above informations supported by linux mipi csi driver also.

Thanks,

P.Ashok

0 件の賞賛
返信

2,588件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ashok

I am afraid current driver does not allow to

provide such debug info. One can try to add this to driver

using attached Linux Manual Chapter 20 MIPI CSI2 Driver.

Best regards

igor

0 件の賞賛
返信