IMX6SX PCIE通信错误

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6SX PCIE通信错误

1,313 Views
lsg5131420
Contributor III

技术支持您好:

         我在使用IMX6SX的PCIE和FPGA通信时出现问题,IMX6SX作为RC,FPGA作为EP。系统可以识别出PCIE设备。但是系统向FPGA内存空间写入数据,在进行读出,发现数据并没有任何变化。具体的操作过程如下:

        root@imx6sx_all:~# lspci

        00:00.0 PCI bridge: Synopsys, Inc. Device abcd (rev 01)

        01:00.0 Memory controller: Xilinx Corporation Default PCIe endpoint ID (rev 26)

        root@imx6sx_all:~# lspci -vvv -s 01:0.0

        01:00.0 Memory controller: Xilinx Corporation Default PCIe endpoint ID (rev 26)

        Subsystem: Xilinx Corporation Default PCIe endpoint ID

        Control: I/O- Mem- BusMaster- SpecCycle- MemWINV- VGASnoop- ParErr+ Stepping- SERR+ FastB2B- DisINTx-

        Status: Cap+ 66MHz- UDF- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- >SERR- <PERR- INTx-

        Interrupt: pin A routed to IRQ 155

        Region 0: Memory at 08100000 (32-bit, non-prefetchable) [disabled] [size=1K]

         

        使用memtool对0x08100000地址进行读写操作,数据没变

         root@imx6sx_all:/unit_tests# ./memtool 08100000=12345678

         Writing 32-bit value 0x12345678 to address 0x08100000

        root@imx6sx_all:/unit_tests# ./memtool 08100000 1      

        E

        Reading 0x1 count starting at address 0x08100000

        0x08100000:  FFFFFFFF

        不知道这么操作是否正确,由于水平所限,很抱歉没能用英文描述。期待您的解答。

0 Kudos
1 Reply

1,065 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Shiguang,

      On how to use PCIe interface, we have a detailed document for linux, see the link, please!

i.MX6Q PCIe EP/RC Validation System

The usage is very similar to yours !

     In additon, you can also refer to this one at the same time:

Freesclae i.MX6 Linux PCIE驱动源码分析 - 小辉辉的日志 - 网易博客

Regards,

Weidong

0 Kudos