iMX6 Local Alpha

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 Local Alpha

1,825 Views
richogrady
Contributor II

We are using local alpha (not in pixel but in a separate buffer) to combine a graphic plane and a video plane in kernel 4.1.15.  Everything works fine except whenever turning local alpha on or off via ioctl MXCFB_SET_LOC_ALPHA, the screen flashes. We tracked this down to mxc_ipuv3_fb.c where the ioctl is handled.  It seems this ioctl will always call the function mxcfb_set_par().  This function basically does a full reinit of fb0 and fb1 and causes the flashing. Turning global alpha on and off does not have such an issue.  Isn't there a cleaner way to turn on local alpha?

Labels (1)
0 Kudos
Reply
1 Reply

1,584 Views
b36401
NXP Employee
NXP Employee

Here is an example for global alpha and local alpha:

https://community.nxp.com/thread/300324

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply