iMX6 - LDB - Display flicker, diagonal print

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 - LDB - Display flicker, diagonal print

Jump to solution
2,329 Views
pierrelgcb
Contributor III

Hello,

I'm using iMX6DL with Android 5.1.1, Linux kernel 3.14.52. I use LVDS output for display signals. These signals are converted to RGB by an external IC because I use RGB display (only LVDS signals are available from iMX6 hardware).

The display orientation is natively portrait.

The display horizontal lines are increasingly vibrating. At the top, screen is well displayed but at the bottom, horizontal lines are going right to left and left to right.

Display Diagonal.JPG

By default, display is printed in diagonal. When I turn on "Show layout bounds", vibration stops. At the left of display, some pixels come from de right of the screen.

Show layout bounds.JPG

Any advice will help.
Thanks, Pierre

Labels (3)
0 Kudos
Reply
1 Solution
2,053 Views
pierrelgcb
Contributor III

Dear Igor,

Problem resolved by hard inverting RGB clock.

Thanks, Pierre

View solution in original post

0 Kudos
Reply
3 Replies
2,053 Views
pierrelgcb
Contributor III

Dear Igor,

Thanks for your advices. I'm working on it. Should takes several days.

Regards, Pierre

0 Kudos
Reply
2,054 Views
pierrelgcb
Contributor III

Dear Igor,

Problem resolved by hard inverting RGB clock.

Thanks, Pierre

0 Kudos
Reply
2,053 Views
igorpadykov
NXP Employee
NXP Employee

Hi Pierre

from description seems there is loss of synchronization, this may be due

to incorrect timings from i.MX6 side (for checking one can try to attach true lvds lcd

with similar characteristics) or rgb converter chip. Later may be caused by poor lvds signal,

for example noise, one can try to diminish it by decreasing cable length and fps.


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply