iMX6 - LDB - Display flicker, diagonal print

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6 - LDB - Display flicker, diagonal print

ソリューションへジャンプ
2,328件の閲覧回数
pierrelgcb
Contributor III

Hello,

I'm using iMX6DL with Android 5.1.1, Linux kernel 3.14.52. I use LVDS output for display signals. These signals are converted to RGB by an external IC because I use RGB display (only LVDS signals are available from iMX6 hardware).

The display orientation is natively portrait.

The display horizontal lines are increasingly vibrating. At the top, screen is well displayed but at the bottom, horizontal lines are going right to left and left to right.

Display Diagonal.JPG

By default, display is printed in diagonal. When I turn on "Show layout bounds", vibration stops. At the left of display, some pixels come from de right of the screen.

Show layout bounds.JPG

Any advice will help.
Thanks, Pierre

ラベル(3)
0 件の賞賛
返信
1 解決策
2,052件の閲覧回数
pierrelgcb
Contributor III

Dear Igor,

Problem resolved by hard inverting RGB clock.

Thanks, Pierre

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,052件の閲覧回数
pierrelgcb
Contributor III

Dear Igor,

Thanks for your advices. I'm working on it. Should takes several days.

Regards, Pierre

0 件の賞賛
返信
2,053件の閲覧回数
pierrelgcb
Contributor III

Dear Igor,

Problem resolved by hard inverting RGB clock.

Thanks, Pierre

0 件の賞賛
返信
2,052件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Pierre

from description seems there is loss of synchronization, this may be due

to incorrect timings from i.MX6 side (for checking one can try to attach true lvds lcd

with similar characteristics) or rgb converter chip. Later may be caused by poor lvds signal,

for example noise, one can try to diminish it by decreasing cable length and fps.


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信