iMX6 GPIO state during Startup & Power Sequencing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX6 GPIO state during Startup & Power Sequencing

跳至解决方案
4,494 次查看
ndsonu
Contributor II

Hello All,

We have a custom board based on i.MX6 (Quad), processor: IMX6 Quad, revision: C. It is powered from PMIC PF0100. We found glitches on few GPIO lines (Ball Name: DI0_PIN2, Ball No: N25) during start up and also noticed that these glitches have relation to power sequencing.

Scenario 1:

Following is the power sequence:

  1. VDDARM_IN, VDDSOC_IN
  2. NVCC_XXX lines
  3. NVCC_DRAM
  4. VDD_SNVS_IN, VDDHIGH_IN

On this sequence we see a glitch (unwanted toggling) on the DI0_PIN2 during start up. Please see the attached waveform

Scenario 2:

Following is the power sequence:

  1. VDD_SNVS_IN
  2. VDDARM_IN, VDDSOC_IN
  3. NVCC_XXX lines, VDDHIGH_IN
  4. NVCC_DRAM

On this sequence we see no glitch but the pin DI0_PIN2  which should be a HIGH due to internal 100K pull up becomes so only after a few milli seconds from RESET.

Scenario 3:

Following is the power sequence:

  1. VDD_SNVS_IN, VDDHIGH_IN
  2. VDDARM_IN, VDDSOC_IN
  3. NVCC_XXX lines,
  4. NVCC_DRAM

On this sequence we see no glitch and pin DI0_PIN2 becomes HIGH before release of RESET.

Observation from above scenarios: VDD_SNVS_IN and VDDHIGH_IN should be applied to i.MX6 before any other supply rails for a glitch free GPIO transitions during reset.

Datasheet says “VDD_SNVS_IN” should be applied first. But I think not anything about “VDDHIGH_IN”.

Is my observation expected?

What is the dependency of GPIO pin on VDD_HIGH_IN?

Thanks in Advance!

Regards,

Sonu Kurian

标签 (1)
1 解答
3,809 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sonu

you are right, scenario 3 provides more glitchless behaviour,

because VDDHIGH_IN provides power for processor control logic.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
3,810 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sonu

you are right, scenario 3 provides more glitchless behaviour,

because VDDHIGH_IN provides power for processor control logic.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

3,809 次查看
ndsonu
Contributor II

Thank You Igor!

0 项奖励
回复