iMX6 Configuration for secure boot failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6 Configuration for secure boot failed

1,485件の閲覧回数
arunkumar_maniv
Contributor III

Hello All,

As per the instructions in the below link,

https://source.codeaurora.org/external/imx/uboot-imx/tree/doc/imx/habv4/guides/mx6_mx7_secure_boot.t...

set CONFIG_SECURE_BOOT=y. Lot of Build errors appeared. Could not spot a particular build error.

Firstly, have enabled in .config file of the u-boot v2017.03. Lot of errors. Then tried to enable via menuconfig, could not locate Secure Boot option in the menuconfig UI. When searched it is visible in the search screen but when selected it goes to the previous sub-menu (ARM-architecture) but then unable to locate secure boot and set it to y.

Please help. Since menuconfig the options are not there I have not attached the build error since the observed build error could be due to updating the inappropriate file (.config).

- Arun

0 件の賞賛
返信
1 返信

1,471件の閲覧回数
Yuri
NXP Employee
NXP Employee

@arunkumar_maniv 
Hello,

   please try to use the same U-boot release as the help - "imx_v2018.03_4.14.78_1.0.0_ga"

Refer to Chapter 3 (Porting U-Boot) of "i.MX_Porting_Guide.pdf" how to build U-boot.

https://www.nxp.com/webapp/Download?colCode=L4.14.78_1.0.0_LINUX_DOCS

 

Regards,
Yuri.

0 件の賞賛
返信