iMX6 Clock Root Generator figures wrong or not?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6 Clock Root Generator figures wrong or not?

ソリューションへジャンプ
2,546件の閲覧回数
MichaelV
Senior Contributor III

Hi,

iMX6SDL/DQ RM section 18.5.1.5.4 Clock Root Generator.

The figures in that chapter show the locations of the Clock Gates. The following signals show no gate (cg) in the figure, but they do have a gate according to the CCGRn registers:

  • PCIE
  • VDO_AXI
  • CAN_CLK
  • UART

Is this a documentation error, or does it mean these signals are really different than the others (maybe gated at a later stage)?

ラベル(4)
0 件の賞賛
返信
1 解決策
2,222件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Michel

correct description is given in CCGRn registers.


Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,223件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Michel

correct description is given in CCGRn registers.


Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,222件の閲覧回数
MichaelV
Senior Contributor III

So, just to confirm; the figures under section 18.5.1.5.4 Clock Root Generator should show (cg) for the PCIE, VD_AXI, CAN_CLK and UART signals? There is nothing "different" with the clock gating than any of the other signals, correct?

0 件の賞賛
返信
2,222件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Yes, correct

Best regards

chip

0 件の賞賛
返信