iMX6 Camera Parallel Interface - BT1120

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 Camera Parallel Interface - BT1120

2,880 Views
lucazini
Contributor I

Hello, I need to read frames from a camera connected to the camera parallel interface of an imx6.

The camera begins to write full hd progressive frames to the parallel interface following the bt1120 standard as soon as the board boots.

I've started to study some v4l2 tutorials and to look for some examples, but I have no experience at all in writing drivers.

I write to ask some help :smileyhappy: A few hints or pointers to useful documentation or a driver I can use as a starting point would be greatly appreciated!

Thanks

0 Kudos
Reply
1 Reply

1,698 Views
joanxie
NXP TechSupport
NXP TechSupport

for bt1120 inprogressive mode, you can refer to the link as below, hope helpful for you.

<Support BT1120 progressive mode in Mx6Q >.

0 Kudos
Reply