iMX6 Cache Errata

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX6 Cache Errata

2,713 次查看
antoine_bardoz
Contributor I

Hi,

Looking at "Chip Errata for the i.MX 6Solo/6DualLite Rev. 7, 04/2019" (IMX6SDLCE.pdf), I have found the following errata which may affect our application:
ERR003739
ERR005198

They reference the following ARM errata numbers:
751470
780370

However, I have been unable to find these in any of the ARM errata documentation for Cortex A9 or PL310. Could you please point me at the source for these errata?

Looking at the errata conditions, and suggested workarounds, it seems to me the only safe way to circumvent these data corruption issues is to use write-through cache. This has a heavy impact on performance, but data corruption must be avoided for us. Am I right in saying this?

I've attached the errata document for your convenience.


Thanks,

Antoine

标记 (3)
0 项奖励
回复
1 回复

2,571 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 

  I've sent You some comments directly.

 

Have a great day,

Yuri

 

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 项奖励
回复