iMX6 - ALSA version supported in Yocto GA release.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX6 - ALSA version supported in Yocto GA release.

跳至解决方案
1,911 次查看
Ansari
Contributor IV

Hi,

We are using imx6Q sabresd platform for our development.  Currently we are working with Linux 3.10.17_1.0.0-GA BSP.

We would like to know,  Which ALSA version is supported in Linux 3.10.17_1.0.0-GA?.

The "cat /proc/asound/version" shows that the ALSA version is k3.10.17-1.0.0_ga+g232293e as mentioned below.

root@imx6qsabresd:~# cat /proc/asound/version

Advanced Linux Sound Architecture Driver Version k3.10.17-1.0.0_ga+g232293e.

Thanks in advance,

Regards,

Ansari

0 项奖励
回复
1 解答
1,359 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Abdul,

please check below

http://freescale.github.io/doc/release-notes/1.6/

fsl-alsa-plugins  - 1.0.25

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,360 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Abdul,

please check below

http://freescale.github.io/doc/release-notes/1.6/

fsl-alsa-plugins  - 1.0.25

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复