iMX6 - ALSA version supported in Yocto GA release.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6 - ALSA version supported in Yocto GA release.

ソリューションへジャンプ
1,916件の閲覧回数
Ansari
Contributor IV

Hi,

We are using imx6Q sabresd platform for our development.  Currently we are working with Linux 3.10.17_1.0.0-GA BSP.

We would like to know,  Which ALSA version is supported in Linux 3.10.17_1.0.0-GA?.

The "cat /proc/asound/version" shows that the ALSA version is k3.10.17-1.0.0_ga+g232293e as mentioned below.

root@imx6qsabresd:~# cat /proc/asound/version

Advanced Linux Sound Architecture Driver Version k3.10.17-1.0.0_ga+g232293e.

Thanks in advance,

Regards,

Ansari

0 件の賞賛
返信
1 解決策
1,364件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Abdul,

please check below

http://freescale.github.io/doc/release-notes/1.6/

fsl-alsa-plugins  - 1.0.25

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,365件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Abdul,

please check below

http://freescale.github.io/doc/release-notes/1.6/

fsl-alsa-plugins  - 1.0.25

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信