iMX6 - ALSA version supported in Yocto GA release.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 - ALSA version supported in Yocto GA release.

Jump to solution
1,930 Views
Ansari
Contributor IV

Hi,

We are using imx6Q sabresd platform for our development.  Currently we are working with Linux 3.10.17_1.0.0-GA BSP.

We would like to know,  Which ALSA version is supported in Linux 3.10.17_1.0.0-GA?.

The "cat /proc/asound/version" shows that the ALSA version is k3.10.17-1.0.0_ga+g232293e as mentioned below.

root@imx6qsabresd:~# cat /proc/asound/version

Advanced Linux Sound Architecture Driver Version k3.10.17-1.0.0_ga+g232293e.

Thanks in advance,

Regards,

Ansari

0 Kudos
Reply
1 Solution
1,378 Views
igorpadykov
NXP Employee
NXP Employee

Hi Abdul,

please check below

http://freescale.github.io/doc/release-notes/1.6/

fsl-alsa-plugins  - 1.0.25

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,379 Views
igorpadykov
NXP Employee
NXP Employee

Hi Abdul,

please check below

http://freescale.github.io/doc/release-notes/1.6/

fsl-alsa-plugins  - 1.0.25

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply