iMX535 Fuse Programming

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX535 Fuse Programming

跳至解决方案
1,407 次查看
sherry_zahid
Contributor III

Hi,

I wanted to know how fuse programming works on the iMX535 (using the "fuse" command in u-boot). Are my following assumptions correct:-

1. If fuse bit(s) are not blown the default value = 0 

2. fuse bit is only blown once you program a value of 1 (and the configuration/fuse retains this value permanently)

I was unable to find this exact information in the ref manual / datasheet.

Thanks
SZ

标签 (2)
标记 (3)
1 解答
1,307 次查看
igorpadykov
NXP Employee
NXP Employee

Hi sherry

1. right

2. right

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,308 次查看
igorpadykov
NXP Employee
NXP Employee

Hi sherry

1. right

2. right

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------