iMX535 Fuse Programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX535 Fuse Programming

ソリューションへジャンプ
1,824件の閲覧回数
sherry_zahid
Contributor III

Hi,

I wanted to know how fuse programming works on the iMX535 (using the "fuse" command in u-boot). Are my following assumptions correct:-

1. If fuse bit(s) are not blown the default value = 0 

2. fuse bit is only blown once you program a value of 1 (and the configuration/fuse retains this value permanently)

I was unable to find this exact information in the ref manual / datasheet.

Thanks
SZ

ラベル(2)
タグ(3)
1 解決策
1,724件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi sherry

1. right

2. right

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,725件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi sherry

1. right

2. right

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------