iMX53 display

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX53 display

1,888件の閲覧回数
lilyliu
Contributor I

Hi All,

I am doing a project will use MCIMX537CVV8B, display will use KOE RGB TX09D40VM3CBA. The LCD dot clk type is 5.6MHz.

I want to know if the CPU could generate the required clock for LCD or need external frequency divider?

Could LCD signal Hsync Vsync DOTCLK connect to CPU directly or need external CPLD? if have any timing sequency issue?


Thanks!


ラベル(2)
0 件の賞賛
返信
1 返信

1,690件の閲覧回数
aven_tsao
NXP Employee
NXP Employee

It is a normal RGB interface LCD panel, MX53 can support it directly without external Timing controller (CPLD).

0 件の賞賛
返信