iMX53 display

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX53 display

1,844 次查看
lilyliu
Contributor I

Hi All,

I am doing a project will use MCIMX537CVV8B, display will use KOE RGB TX09D40VM3CBA. The LCD dot clk type is 5.6MHz.

I want to know if the CPU could generate the required clock for LCD or need external frequency divider?

Could LCD signal Hsync Vsync DOTCLK connect to CPU directly or need external CPLD? if have any timing sequency issue?


Thanks!


标签 (2)
0 项奖励
回复
1 回复

1,646 次查看
aven_tsao
NXP Employee
NXP Employee

It is a normal RGB interface LCD panel, MX53 can support it directly without external Timing controller (CPLD).

0 项奖励
回复