iMX53 display

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX53 display

1,886 Views
lilyliu
Contributor I

Hi All,

I am doing a project will use MCIMX537CVV8B, display will use KOE RGB TX09D40VM3CBA. The LCD dot clk type is 5.6MHz.

I want to know if the CPU could generate the required clock for LCD or need external frequency divider?

Could LCD signal Hsync Vsync DOTCLK connect to CPU directly or need external CPLD? if have any timing sequency issue?


Thanks!


Labels (2)
0 Kudos
Reply
1 Reply

1,688 Views
aven_tsao
NXP Employee
NXP Employee

It is a normal RGB interface LCD panel, MX53 can support it directly without external Timing controller (CPLD).

0 Kudos
Reply