iMX53 Quick Start Board with EasyCap USB Camera Support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX53 Quick Start Board with EasyCap USB Camera Support

1,872件の閲覧回数
Saminath
Contributor I

Hi,

   I have iMX53 QSB. Linux is up and Running on the Board. I wish to interface QSB with EASY CAP Usb camera to capture the Image.

Linux is able to detect the USB Camera device and it creates video device node.  If I run the Capture.c application then i got  'Select Time Out Error' .

Kindly advice me , what i am missing.

thanks,

saminath

タグ(1)
0 件の賞賛
返信
0 返答(返信)