Host Controller Interface issue in IMX53 QSB android 2.3.4

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Host Controller Interface issue in IMX53 QSB android 2.3.4

1,139 次查看
swaraj
Contributor II

Hi,

    I downloaded gingerbread android 2.3.4 and 2.6.35.3 kernel. I have built that android version for IMX53 QSB and I'm using a SDIO supported WIFI card in the SDIO slot provided in IMX53 QSB. I have a problem in sending data down to the device. The packet for which I issue a cmd53 write (packet size: 256) has some non-zero bytes in it. However, when the packet reaches the device, the data somehow gets corrupted and I get to see zeroes instead of valid data.

Can anyone please help in resolving this issue.

Thanks
Swaraj

标签 (1)
标记 (2)
0 项奖励
回复
0 回复数