iMX53 Quick Start Board with EasyCap USB Camera Support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX53 Quick Start Board with EasyCap USB Camera Support

1,874 次查看
Saminath
Contributor I

Hi,

   I have iMX53 QSB. Linux is up and Running on the Board. I wish to interface QSB with EASY CAP Usb camera to capture the Image.

Linux is able to detect the USB Camera device and it creates video device node.  If I run the Capture.c application then i got  'Select Time Out Error' .

Kindly advice me , what i am missing.

thanks,

saminath

标记 (1)
0 项奖励
回复
0 回复数