iMX51 boot failures

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX51 boot failures

1,707件の閲覧回数
SteM
Contributor III

Hi @all,
iMX51 board booting WinCE600R3, BSP based on Freescale one.
We enabled the registry hive and ROM+RAM FS.

If i save the registry into a folder in RAM [SDMemory MountAsBootable=0 MountAsRoot=0, ObjectStore MountAsBootable=1 MountAsRoot=1] (even if it is hive registry), i have no problem.

If i change the settings to save the registry into SdMemory [SDMemory MountAsBootable=1 MountAsRoot=0, and ObjectStore MountAsBootable=0 MountAsRoot=1] my image sometimes run, sometimes stop with the message:
FILESYS: Waiting for bootable file system to be mounted.

The percentage of failure is almost 50%.
If I lower the frequency into the bootloader to 7.5MHz, the percentage is low but there are too many times with the problem.

Please, have you any advise/application note/doc to solve this problem??

Thanks

タグ(1)
0 件の賞賛
返信
3 返答(返信)

1,214件の閲覧回数
qiang_li-mpu_se
NXP Employee
NXP Employee

Attached is an example to enable BINFS, HIVEREG and ROM only filesystem on SDMMC card, BSP is based on WINCE5.0 ER1104 IMX51 BSP. Maybe you can reference to it for your HIVEREG case.

0 件の賞賛
返信

1,214件の閲覧回数
huzizhen
Contributor I

hi Liqiang:

     I have a same program to use hive-base registy for wince6 on imx51.when i set ,i can not boot. i see your reply, so i want to test it .

     I used your Attach files to build a bin.and download it by mfgtool  sucessed .but when it boot,many error msg and can not into wince os .pls give me some advice. and i only modifty IMGCOMPRESSALL=1 because your files not set.

and your readme have some msg: xip.nb0 and eboot.nb0 are instead of nk.nb0 and eboot.nb0 and xldr.nb0.

but your ucl.xml still have xldr.nb0 to download to sdmmc,why?

the attach files is my config.

see follow msg.

Freescale iMX SOC Menu Item   (UNSAVED CHANGES)

-----------------------------------------------------------------------------

[0] IP Address : 0.0.0.0

[1] Set IP Mask : 0.0.0.0

[2] Boot Delay : 3

[3] DHCP : Enabled

[4] Reset to Factory Default Configuration

[5] Select Boot Device : NK from SD/MMC

[6] Set MAC Address : FF-FF-FF-FF-FF-FF

[7] Format OS NAND Region

[8] Format All NAND Regions

[9] Bootloader Shell

[I] KITL Work Mode : Interrupt

[K] KITL Enable Mode : Disable

[P] KITL Passive Mode : Disable

[S] Save Settings

[D] Download Image Now

[L] Launch Existing Flash Resident Image Now

[E] Select Ether Device : FEC

[M] MMC and SD Utilities

Selection: l

INFO: Storing boot configuration to SDHC

INFO: Successfully stored boot configuration to SDHC

-BLMenu .

INFO: Using device name: 'MX5165535'

INFO: Reading NK image to SDHC (please wait)...

Card Capacity 1967616 (Kbytes)

Successfully created 3 partitions

Boot Partition size = 767 Kbytes, startSect = 0x2, totSect = 0x5fe.

BINFS Partition size = 32768 Kbytes, startSect = 0x600, totSect = 0x10000

File System Partition size = 1934080 Kbytes, startSect = 0x10600, totSect = 0x3b0600

INFO: Copying NK image to RAM address 0xa0200000

INFO: Copying NK image size 0x300000 BYTEs.

INFO: Read is 8% complete

INFO: Read is 16% complete

INFO: Read is 25% complete

INFO: Read is 33% complete

INFO: Read is 41% complete

INFO: Read is 50% complete

INFO: Read is 58% complete

INFO: Read is 66% complete

INFO: Read is 75% complete

INFO: Read is 83% complete

INFO: Read is 91% complete

INFO: Read is 100% complete

INFO: Copy of NK completed successfully

Download successful!  Jumping to image at 0x0 (physical 0x90200000)...

INFO:OALLogSetZones: dpCurSettings.ulZoneMask: 0xb

BSP Clock Configuration:

    CKIH        =   22579200 Hz

    PLL1        =  800000000 Hz

    PLL2        =  665000000 Hz

    PLL3        =  216000000 Hz

    LP_APM      =   24000000 Hz

    ARM         =  800000000 Hz

    AXI_A       =  166250000 Hz

    AXI_B       =  133000000 Hz

    EMI_SLOW    =  133000000 Hz

    AHB         =  133000000 Hz

    IPG         =   66500000 Hz

    PERCLK      =    8000000 Hz

    CKIL_SYNC   =      32768 Hz

    DDR         =  200000000 Hz

    ARM_AXI     =  166250000 Hz

    IPU_HSP     =  133000000 Hz

    VPU_AXI     =  166250000 Hz

    GPU         =  166250000 Hz

    GPU2D       =  166250000 Hz

    DEBUG_APB   =  166250000 Hz

    ENFC        =   26600000 Hz

    USBOH3      =   66500000 Hz

    ESDHC1      =   47500000 Hz

    ESDHC2      =   47500000 Hz

    ESDHC3      =   47500000 Hz

    ESDHC4      =   47500000 Hz

    UART        =   24000000 Hz

    SSI1        =    5644800 Hz

    SSI2        =    5644800 Hz

    SSI3        =    5644800 Hz

    SSI_EXT1    =   10285714 Hz

    SSI_EXT2    =   10285714 Hz

    USB_PHY     =   24000000 Hz

    TVE_216_54  =  216000000 Hz

    DI          =   27000000 Hz

    VPU_RCLK    =   24000000 Hz

    SPDIF0      =    1142857 Hz

    SPDIF1      =    1142857 Hz

    SLIMBUS     =   66500000 Hz

    SIM         =   66500000 Hz

    FIRI        =   24000000 Hz

    HSI2C       =   66500000 Hz

    SSI_LP_APM  =   22579200 Hz

    SPDIF_XTAL  =   24000000 Hz

    HSC1        =  216000000 Hz

    HSC2        =  216000000 Hz

    ESC         =   15428571 Hz

    CSI_MCLK1   =   24629629 Hz

    CSI_MCLK2   =   24629629 Hz

    ECSPI       =   66500000 Hz

    LPSR        =          0 Hz

    PGC         =   66500000 Hz

    OSC         =   24000000 Hz

    CKIH_CAMP1  =   22579200 Hz

    CKIH2_CAMP2 =          0 Hz

    CKIH2       =          0 Hz

    FPM         =   33554432 Hz

Windows CE Kernel for ARM (Thumb Enabled) Built on May  7 2012 at 12:47:43

INFO:OALLogSetZones: dpCurSettings.ulZoneMask: 0xb

+OEMInit

OEMInit:  silicon rev = 0x20

BoardID = 0x0.

+OEMInit before kitl init,fffc7ffd,ffffffff

[KITL] ++OALKitlInit()hu

pDevice->type............ 2

WARN: OALKitlInit: KITL Disabled

OALIoCtlHalInitRTC(2006/1/1 12:0:0.000)

Exception 'Data Abort' (4): Thread-Id=00610002(pth=9bfa4420), Proc-Id=00400002(pprc=8055b308) 'NK.EXE', VM-active=00400002(pprc=8055b308) 'NK.EXE'

PC=c00bc6f8(k.coredll.dll+0x0002c6f8) RA=c00d11e8(k.coredll.dll+0x000411e8) SP=d00bfac0, BVA=00000000

Exception 'Data Abort' (4): Thread-Id=00610002(pth=9bfa4420), Proc-Id=00400002(pprc=8055b308) 'NK.EXE', VM-active=00400002(pprc=8055b308) 'NK.EXE'

PC=c00bc6f8(k.coredll.dll+0x0002c6f8) RA=c00d11e8(k.coredll.dll+0x000411e8) SP=d00bfac0, BVA=00000000

OALIoCtlHalInitRTC(2006/1/1 12:0:0.000)

Exception 'Data Abort' (4): Thread-Id=00610002(pth=9bfa4420), Proc-Id=00400002(pprc=8055b308) 'NK.EXE', VM-active=00400002(pprc=8055b308) 'NK.EXE'

PC=c00bc6f8(k.coredll.dll+0x0002c6f8) RA=c00d11e8(k.coredll.dll+0x000411e8) SP=d00bfac0, BVA=00000000

Exception 'Data Abort' (4): Thread-Id=00610002(pth=9bfa4420), Proc-Id=00400002(pprc=8055b308) 'NK.EXE', VM-active=00400002(pprc=8055b308) 'NK.EXE'

PC=c00bc6f8(k.coredll.dll+0x0002c6f8) RA=c00d11e8(k.coredll.dll+0x000411e8) SP=d00bfac0, BVA=00000000

OALIoCtlHalInitRTC(2006/1/1 12:0:0.000)

Exception 'Data Abort' (4): Thread-Id=00610002(pth=9bfa4420), Proc-Id=00400002(pprc=8055b308) 'NK.EXE', VM-active=00400002(pprc=8055b308) 'NK.EXE'

PC=c00bc6f8(k.coredll.dll+0x0002c6f8) RA=c00d11e8(k.coredll.dll+0x000411e8) SP=d00bfac0, BVA=00000000

Exception 'Data Abort' (4): Thread-Id=00610002(pth=9bfa4420), Proc-Id=00400002(pprc=8055b308) 'NK.EXE', VM-active=00400002(pprc=8055b308) 'NK.EXE'

PC=c00bc6f8(k.coredll.dll+0x0002c6f8) RA=c00d11e8(k.coredll.dll+0x000411e8) SP=d00bfac0, BVA=00000000

OALIoCtlHalInitRTC(2006/1/1 12:0:0.000)

Exception 'Data Abort' (4): Thread-Id=00610002(pth=9bfa4420), Proc-Id=00400002(pprc=8055b308) 'NK.EXE', VM-active=00400002(pprc=8055b308) 'NK.EXE'

PC=c00bc6f8(k.coredll.dll+0x0002c6f8) RA=c00d11e8(k.coredll.dll+0x000411e8) SP=d00bfac0, BVA=00000000

Exception 'Data Abort' (4): Thread-Id=00610002(pth=9bfa4420), Proc-Id=00400002(pprc=8055b308) 'NK.EXE', VM-active=00400002(pprc=8055b308) 'NK.EXE'

PC=c00bc6f8(k.coredll.dll+0x0002c6f8) RA=c00d11e8(k.coredll.dll+0x000411e8) SP=d00bfac0, BVA=00000000

OALIoCtlHalInitRTC(2006/1/1 12:0:0.000)

Exception 'Data Abort' (4): Thread-Id=00610002(pth=9bfa4420), Proc-Id=00400002(pprc=8055b308) 'NK.EXE', VM-active=00400002(pprc=8055b308) 'NK.EXE'

PC=c00bc6f8(k.coredll.dll+0x0002c6f8) RA=c00d11e8(k.coredll.dll+0x000411e8) SP=d00bfac0, BVA=00000000

Exception 'Data Abort' (4): Thread-Id=00610002(pth=9bfa4420), Proc-Id=00400002(pprc=8055b308) 'NK.EXE', VM-active=00400002(pprc=8055b308) 'NK.EXE'

PC=c00bc6f8(k.coredll.dll+0x0002c6f8) RA=c00d11e8(k.coredll.dll+0x000411e8) SP=d00bfac0, BVA=00000000

OALIoCtlHalInitRTC(2006/1/1 12:0:0.000)

Exception 'Data Abort' (4): Thread-Id=00610002(pth=9bfa4420), Proc-Id=00400002(pprc=8055b308) 'NK.EXE', VM-active=00400002(pprc=8055b308) 'NK.EXE'

PC=c00bc6f8(k.coredll.dll+0x0002c6f8) RA=c00d11e8(k.coredll.dll+0x000411e8) SP=d00bfac0, BVA=00000000

Exception 'Data Abort' (4): Thread-Id=00610002(pth=9bfa4420), Proc-Id=00400002(pprc=8055b308) 'NK.EXE', VM-active=00400002(pprc=8055b308) 'NK.EXE'

PC=c00bc6f8(k.coredll.dll+0x0002c6f8) RA=c00d11e8(k.coredll.dll+0x000411e8) SP=d00bfac0, BVA=00000000

OALIoCtlHalInitRTC(2006/1/1 12:0:0.000)

Exception 'Data Abort' (4): Thread-Id=00610002(pth=9bfa4420), Proc-Id=00400002(pprc=8055b308) 'NK.EXE', VM-active=00400002(pprc=8055b308) 'NK.EXE'

PC=c00bc6f8(k.coredll.dll+0x0002c6f8) RA=c00d11e8(k.coredll.dll+0x000411e8) SP=d00bfac0, BVA=00000000

Exception 'Data Abort' (4): Thread-Id=00610002(pth=9bfa4420), Proc-Id=00400002(pprc=8055b308) 'NK.EXE', VM-active=00400002(pprc=8055b308) 'NK.EXE'

PC=c00bc6f8(k.coredll.dll+0x0002c6f8) RA=c00d11e8(k.coredll.dll+0x000411e8) SP=d00bfac0, BVA=00000000

OALIoCtlHalInitRTC(2006/1/1 12:0:0.000)

Exception 'Data Abort' (4): Thread-Id=00610002(pth=9bfa4420), Proc-Id=00400002(pprc=8055b308) 'NK.EXE', VM-active=00400002(pprc=8055b308) 'NK.EXE'

PC=c00bc6f8(k.coredll.dll+0x0002c6f8) RA=c00d11e8(k.coredll.dll+0x000411e8) SP=d00bfac0, BVA=00000000

Exception 'Data Abort' (4): Thread-Id=00610002(pth=9bfa4420), Proc-Id=00400002(pprc=8055b308) 'NK.EXE', VM-active=00400002(pprc=8055b308) 'NK.EXE'

PC=c00bc6f8(k.coredll.dll+0x0002c6f8) RA=c00d11e8(k.coredll.dll+0x000411e8) SP=d00bfac0, BVA=00000000

OALIoCtlHalInitRTC(2006/1/1 12:0:0.000)

Exception 'Data Abort' (4): Thread-Id=00610002(pth=9bfa4420), Proc-Id=00400002(pprc=8055b308) 'NK.EXE', VM-active=00400002(pprc=8055b308) 'NK.EXE'

PC=c00bc6f8(k.coredll.dll+0x0002c6f8) RA=c00d11e8(k.coredll.dll+0x000411e8) SP=d00bfac0, BVA=00000000

Exception 'Data Abort' (4): Thread-Id=00610002(pth=9bfa4420), Proc-Id=00400002(pprc=8055b308) 'NK.EXE', VM-active=00400002(pprc=8055b308) 'NK.EXE'

PC=c00bc6f8(k.coredll.dll+0x0002c6f8) RA=c00d11e8(k.coredll.dll+0x000411e8) SP=d00bfac0, BVA=00000000

OALIoCtlHalInitRTC(2006/1/1 12:0:0.000)

Exception 'Data Abort' (4): Thread-Id=00610002(pth=9bfa4420), Proc-Id=00400002(pprc=8055b308) 'NK.EXE', VM-active=00400002(pprc=8055b308) 'NK.EXE'

PC=c00bc6f8(k.coredll.dll+0x0002c6f8) RA=c00d11e8(k.coredll.dll+0x000411e8) SP=d00bfac0, BVA=00000000

Exception 'Data Abort' (4): Thread-Id=00610002(pth=9bfa4420), Proc-Id=00400002(pprc=8055b308) 'NK.EXE', VM-active=00400002(pprc=8055b308) 'NK.EXE'

PC=c00bc6f8(k.coredll.dll+0x0002c6f8) RA=c00d11e8(k.coredll.dll+0x000411e8) SP=d00bfac0, BVA=00000000

OALIoCtlHalInitRTC(2006/1/1 12:0:0.000)

Exception 'Data Abort' (4): Thread-Id=00610002(pth=9bfa4420), Proc-Id=00400002(pprc=8055b308) 'NK.EXE', VM-active=00400002(pprc=8055b308) 'NK.EXE'

PC=c00bc6f8(k.coredll.dll+0x0002c6f8) RA=c00d11e8(k.coredll.dll+0x000411e8) SP=d00bfac0, BVA=00000000

Exception 'Data Abort' (4): Thread-Id=00610002(pth=9bfa4420), Proc-Id=00400002(pprc=8055b308) 'NK.EXE', VM-active=00400002(pprc=8055b308) 'NK.EXE'

PC=c00bc6f8(k.coredll.dll+0x0002c6f8) RA=c00d11e8(k.coredll.dll+0x000411e8) SP=d00bfac0, BVA=00000000

OALIoCtlHalInitRTC(2006/1/1 12:0:0.000)

0 件の賞賛
返信

1,214件の閲覧回数
qiang_li-mpu_se
NXP Employee
NXP Employee

xldr.nb0 has no change, it still be used to load the eboot.nb0.

0 件の賞賛
返信