Hi all,
I download [imx-android-r10.4_bundle_BSP.tar.gz] from Freescale website and follow its user guide [i.MX Android R10.4 User Guide].
I am trying to build a u-boot image by myself. So I follow all the steps of source code download like below.
$ cd myandroid/bootable/bootloader
$ git clone git://git.denx.de/u-boot.git uboot-imx
After [uboot-imx] folder download finish. And finish apply R10.4 release patch.
Then I try to follow below steps and caused an Error message below. I found there is no string [mx51_bbg_android_config] in makefile. and related mx51_bbg_android file such as mx51_bbg_android.h in [uboot-imx] folder. Which steps I missed? Please help me. Thank you.
$ cd ~/myandroid/bootable/bootloader/uboot-imx
$ export ARCH=arm
$ export CROSS_COMPILE=~/myandroid/prebuilt/linux-x86/toolchain/arm-eabi-4.3.1/bin/arm-eabi-
Command to build for i.MX51 BBG board is:
$ make distclean
$ make mx51_bbg_android_config
$ make
Error message:
make: *** No rule to make target `mx51_bbg_android_config'. Stop.
Sorry, I found out the correct name.
$ make mx51_defconfig
Now I am checking how to build Android image with correct product name.
$lunch imx51_bbg-user
Error message:
build/core/product_config.mk:203: *** No matches for product "imx51_bbg". Stop.
** Don't have a product spec for: 'imx51_bbg'
** Do you have the right repo manifest?
I am not an Android guy so I won't be able to help here.
Thank you Otavio. But here I face a boot problem. After I build u-boot.bin and uImage. I flash in my SD card and try to boot MX51 EVK board. It cannot boot-up. I don't know what's wrong. Can you give me some advice?
Here is my SD card partition status:
| Device Boot | Start | End | Blocks Id System | |
| /dev/sdb1 | 19532 | 13949064 | 6964766+ 83 Linux | |
| /dev/sdb2 | 13949065 | 14925664 | 488300 83 Linux | |
| /dev/sdb3 | 14925665 | 15925664 | 500000 | 5 Extended |
| /dev/sdb4 | 15925665 | 16019455 | 46895+ 83 Linux | |
| /dev/sdb5 | 14927713 | 15806653 | 439470+ 83 Linux | |
| /dev/sdb6 | 15808702 | 15925664 | 58481+ 83 Linux |
Flash u-boot-no-padding.bin command:
$ sudo dd if=u-boot-no-padding.bin of=/dev/sdb bs=1K seek=1; sync
Result:
301+1 records in
301+1 records out
308864 bytes (309 kB) copied, 0.103723 s, 3.0 MB/s
Flash uImage command:
$ sudo dd if=uImage of=/dev/sdb bs=1M seek=1; sync
Result:
1+1 records in
1+1 records out
1897828 bytes (1.9 MB) copied, 0.00358143 s, 530 MB/s
What is the log, in serial console?
It could well be it; I'd test the Yocto built image as I know it works.
Double check the u-boot repo. I don’t have the documentation at hand, but it can be this git://git.freescale.com/imx/uboot-imx.git