Hi Manjunath
this is provided by HW_PINCTRL_DOEx register, from
sect.9.4.53 PINCTRL Bank 0 Data Output Enable Register
(HW_PINCTRL_DOE0) MCIMX28RM
For pins in bank 0 that are configured as GPIOs, a 1 in this register will enable the
corresponding bit value from HW_PINCTRL_DOUTxx register to be driven out the pin,
and a 0 in this register will disable the corresponding driver.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------