iMX280 GPIO configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX280 GPIO configuration

905件の閲覧回数
manjunathdn
Contributor I

How can we drive the GPIO's of iMX280 to high impedance or tri-state? Can someone provide details of the GPIO configuration / settings?

ラベル(1)
0 件の賞賛
返信
1 返信

828件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Manjunath

this is provided by HW_PINCTRL_DOEx register, from

sect.9.4.53 PINCTRL Bank 0 Data Output Enable Register

(HW_PINCTRL_DOE0) MCIMX28RM

For pins in bank 0 that are configured as GPIOs, a 1 in this register will enable the

corresponding bit value from HW_PINCTRL_DOUTxx register to be driven out the pin,

and a 0 in this register will disable the corresponding driver.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信