iMX28 emulation on QEMU?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX28 emulation on QEMU?

2,593 Views
CodeWarrior4_2M
Contributor II

Is it possible to run the same instance of the Linux kernel running available on iMX28 platfrom on QEMU environment? Is there a specific Linux release for the iMX28 platform?

Labels (2)
0 Kudos
Reply
1 Reply

1,721 Views
igorpadykov
NXP Employee
NXP Employee

Hi 79 RPM

I think yes, FSL does not provide on iMX28 QEMU, however one can look in web like below 

Booting Linux with U-Boot on QEMU ARM | Freedom Embedded

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply