SabreSD ENET_REF_CLK AC coupling

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SabreSD ENET_REF_CLK AC coupling

跳至解决方案
1,763 次查看
mahi
Contributor IV

Hi community,

is there another reason for AC coupling at the ENET_REF_CLK input in SabreSD-design than adjusting the voltage levels?

In my design I want to use 2.5V for all the Ethernet-related stuff (NVCC_ENET, NVCC_RGMII and VDDIO of the PHY) so connecting ENET_REF_CLK directly (only with a series resistor at the PHY's output) should be OK - or did I miss something?

Best regards,

Martin

标签 (4)
标记 (2)
0 项奖励
回复
1 解答
1,579 次查看
igorpadykov
NXP Employee
NXP Employee

HI Martin

I agree with you: with the same voltage for all the Ethernet-related stuff

connecting ENET_REF_CLK directly is OK.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,580 次查看
igorpadykov
NXP Employee
NXP Employee

HI Martin

I agree with you: with the same voltage for all the Ethernet-related stuff

connecting ENET_REF_CLK directly is OK.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复