iMX28 : PWM output pin behavior

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX28 : PWM output pin behavior

ソリューションへジャンプ
1,357件の閲覧回数
koichisakagami
Contributor II

Dear community,

We design the custom board .
We need information about PWM output pin behavior.

After the PWM register setting is completed,
we disable a PWM channel_xx by the PWM Control and Status Register (:PWMxx_ENABLE => 0).

Question1.
Then, What is the PWM output state ?
Is it high impedance ?

Question2.
    Then, Can the internal keeper be enabled / disabled separately ?

Best Regards,
Koichi Sakagami

ラベル(1)
0 件の賞賛
返信
1 解決策
1,255件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi koichi

1. yes it is high impedance

2. this can be done for some pads (not all), check

HW_PINCTRL_PULLx register descriptions.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,256件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi koichi

1. yes it is high impedance

2. this can be done for some pads (not all), check

HW_PINCTRL_PULLx register descriptions.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信