iMX25-Nand boot error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX25-Nand boot error

1,311 次查看
arumugamramasam
Contributor II

Hi,

I am using iMX25 PDK with Nand flash as boot source.

 

I have my LTIB set for jffs2 as target image and the output of the ./ltib command generates the above files which I copied in to Flash.

 

I have loaded the u-boot.bin, uImage and rootfs.jffs2 files using ATK tool at 0x00000000, 0x00300000 & 0x00800000 respectively. When booting first time, I have changed the bootargs and bootcmd to boot from nand flash. After that my system boots and throws an Kernel panic error. Need support in finding the root cause for this kernel panic.

 

Log is attached.

 

 

 

Thanks,

Arumugam R

Original Attachment has been moved to: NandBoot_KernelPanic.txt.zip

标签 (1)
0 项奖励
回复
0 回复数