iMX233 USB connection mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX233 USB connection mode

1,432 次查看
paolomartinetti
Contributor I

Hi everybody.

i have some problem with my device, 233-equipped, when i plug USB cable first on computer and after in device.

The device-plug probably connects D+/ D- pins before power and ground ones.

Could be this wrong? After this 'bad' connection, my device stops working and seems powered off.

Is there any way to avoid this acting on kernel code?

Thanks in advance

0 项奖励
回复
3 回复数

1,309 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Paolo

it is not allowed to apply voltages to unpowered processor.

This can not be configured in software.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,309 次查看
paolomartinetti
Contributor I

My device is powered with a Li-Ion battery. I attach USB connecting data pins before Power and Ground pins.

0 项奖励
回复

1,309 次查看
igorpadykov
NXP Employee
NXP Employee

it does not matter, if processor is not turned on

(unpowered)

Power-up can be started with one of several events:

PSWITCH pin >= minimum MID level PSWITCH for 100 ms

VDD5V power pin > 4.25 V for 100 ms

0 项奖励
回复