iMX mini uboot hangs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX mini uboot hangs

3,278件の閲覧回数
kajolkharbanda
NXP Employee
NXP Employee

i am trying to access PCI address space in imx8mmevk board using md command,

the u-boot hangs after typing this command,

i was expecting to see the device id and vendor id as this is PCI base address

 

u-boot # md  0x33800000

is it not possible to see the PCI address space using read command from u-boot.

 

0 件の賞賛
返信
6 返答(返信)

3,265件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

I checked the uboot source code, it seems uboot doesn't enable pcie, you can use memtool in the kernel when board boot up to read the register

0 件の賞賛
返信

3,254件の閲覧回数
kajolkharbanda
NXP Employee
NXP Employee

i need to access the pci from u-boot.

Can i enable PCI from u-boot ?

0 件の賞賛
返信

3,243件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

check the mail pls

0 件の賞賛
返信

3,238件の閲覧回数
kajolkharbanda
NXP Employee
NXP Employee

Thanks, how to build u-boot and flash it ?

0 件の賞賛
返信

3,222件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

you can use uuu tools or dd command to flash uboot to the emmc or sd card, more detailed information, pls refer to the user guide

0 件の賞賛
返信

3,117件の閲覧回数
kajolkharbanda
NXP Employee
NXP Employee

the uboot patch you gave me seems to be incompatible with my BSP 

i.MX Linux Yocto Project BSP 6.1.22_2.0.0 Release

0 件の賞賛
返信