Hi Team,
Currently Iam working on imx53qsb , looking to calibrate the touch screen using xinput-calibrator or weston-init but iam unable to get support for either of them.
Kernel version: 6.1
Yocto - Kirkstone
Distro-poky
1. when I add weston or weston-init to local.conf using IMAGE_INSTALL:append, It shows below error
ERROR: Nothing RPROVIDES 'weston-init' (but poky/meta/recipes-extended/images/core-image-full-cmdline.bb RDEPENDS on or otherwise requires it)
weston-init was skipped: missing required distro feature 'pam' (not in DISTRO_FEATURES)
NOTE: Runtime target 'weston-init' is unbuildable, removing...
Missing or unbuildable dependency chain was: ['weston-init']
2.When i run xinput-claibrator after building , it shows the error "Unable to connect to X server".
I have exported display command also
Please help me to calibrate the touch screen with any of this methods