iMX mini uboot hangs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX mini uboot hangs

947 Views
kajolkharbanda
NXP Employee
NXP Employee

i am trying to access PCI address space in imx8mmevk board using md command,

the u-boot hangs after typing this command,

i was expecting to see the device id and vendor id as this is PCI base address

 

u-boot # md  0x33800000

is it not possible to see the PCI address space using read command from u-boot.

 

0 Kudos
Reply
6 Replies

934 Views
joanxie
NXP TechSupport
NXP TechSupport

I checked the uboot source code, it seems uboot doesn't enable pcie, you can use memtool in the kernel when board boot up to read the register

0 Kudos
Reply

923 Views
kajolkharbanda
NXP Employee
NXP Employee

i need to access the pci from u-boot.

Can i enable PCI from u-boot ?

0 Kudos
Reply

912 Views
joanxie
NXP TechSupport
NXP TechSupport

check the mail pls

0 Kudos
Reply

907 Views
kajolkharbanda
NXP Employee
NXP Employee

Thanks, how to build u-boot and flash it ?

0 Kudos
Reply

891 Views
joanxie
NXP TechSupport
NXP TechSupport

you can use uuu tools or dd command to flash uboot to the emmc or sd card, more detailed information, pls refer to the user guide

0 Kudos
Reply

786 Views
kajolkharbanda
NXP Employee
NXP Employee

the uboot patch you gave me seems to be incompatible with my BSP 

i.MX Linux Yocto Project BSP 6.1.22_2.0.0 Release

0 Kudos
Reply