Hi Team,
We are currently working with the NXP Config Tools for i.MX95 DDR configuration and are facing an issue while generating the DDR initialization/timing code.
We created/opened the DDR configuration for the following target:
- Processor: MIMX9596xxxxN
- Core: Cortex-M33
- Memory Type: LPDDR5 - Ryzen RS2G32LO5D4FDB-23BT
- DDR Data Rate: 6400 MT/s
- Number of Ranks: 2
- Number of 16-bit Channels: 2
- DRAM Configuration: 16Gb:2Gb x8
- Total DRAM Density shown by the tool: 16384 MB
Initially, we are trying to validate the DDR configuration using the NXP i.MX95 19x19 EVK default LPDDR5 configuration before applying our custom board DDR settings.
However, when we try to generate/update the DDR code, the Config Tools reports an error in the Problems window:
“Failed to generate code…”
and the Code Preview window shows:
“Code generation failed.”
The screenshot of the issue is attached for reference: