i2s format and PCM format

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i2s format and PCM format

Jump to solution
27,626 Views
jamesdeepu
Contributor II

Can someone explain what is the difference between I2S interface and PCM interface. Does I2S interface only supports i2s format audio data and not PCM format audio data ?

Labels (3)
Tags (5)
1 Solution
6,871 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Basically : I2S is interface, PCM is a digital representation of an audio signal.
"I2S, also known as Inter-IC Sound, Integrated Interchip Sound, or IIS, is an electrical serial bus
interface standard used for connecting digital audio devices together. It is used to communicate PCM
audio data between integrated circuits in an electronic device."


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

3 Replies
6,872 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Basically : I2S is interface, PCM is a digital representation of an audio signal.
"I2S, also known as Inter-IC Sound, Integrated Interchip Sound, or IIS, is an electrical serial bus
interface standard used for connecting digital audio devices together. It is used to communicate PCM
audio data between integrated circuits in an electronic device."


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

6,871 Views
jamesdeepu
Contributor II

Dear Yuri,

Thanks for your reply.!!..

So there is nothing like PCM interface ?

Can you explain I2S audio format too?

Thanks in advance.

0 Kudos
Reply
6,871 Views
Yuri
NXP Employee
NXP Employee

Hi,

Please look at sections 3.1 (General PCM Codec)  and 3.2 (I2S) of the following

app note :

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN2979.pdf

Regards,

Yuri.

0 Kudos
Reply